CMPx.MODVALUE
Description
Use this keyword to read the modulo value.
General Information
|
Type |
R/O Parameter |
|
Units |
Units depend on value of CMPx.SOURCE. See table below. |
|
Range |
-9,223,372,036,854,775,808 to 9,223,372,036,854,775,808 |
|
Default Value |
9,223,372,036,854,775,808 |
|
Data Type |
Integer |
|
Start Version |
M_01-13-00-000 |
Units
| CMPx.SOURCE | Units |
|---|---|
| 0 (FB1) | Depends on FB1.PUNIT or custom units. |
| 1 (FB2) | Depends on FB2.PUNIT or custom units. |
| 2 (FB3) | Depends on FB2.PUNIT or custom units. |
| 3 (PL.FB) | Depends on UNIT.PLINEAR
or UNIT.PROTARY
Rotary: counts, rad, deg, (custom units), 16-bit counts Linear: counts, mm, µm, (custom units), 16-bit counts |
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| AKD PDMM | Revision DB or higher |
| AKD-T-IC |
Revision DA or higher |
| Fieldbus |
Index/Subindex | Object Start Version | |
|---|---|---|---|
| 34A8h/0 |
CMP0.MODVALUE |
M_01-13-00-000 | |
| 34B8h/0 |
CMP1.MODVALUE |
||
Related Topics
|
Copyright © 2018 Kollmorgen |
|