CMPx.OUTMASK

Description

This keyword sets the binary output disable mask between the setpointClosedSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach and the drive's output pin. Note the internal setpoint state remains valid, only the external output is blocked.

Example

The following example sets an outmask to 7 (binary 111) to block setpoint states 0, 1, and 2 from asserting the drive output pin.

-->CMP0.OUTMASK 7

General Information

Type

NV Parameter

Units

None

Range

0 to 255

Default Value

0 (Inactive)

Data Type

Integer

Start Version

M_01-13-00-000

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
AKD PDMM Revision DB or higher
AKD-T-ICClosed"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material Revision DA or higher
FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5394h/0

CMP0.OUTMASK

M_01-13-00-000
539Bh/0

CMP1.OUTMASK

Related Topics

Compare Engines

CMPx.SETPOINT

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen