DRV.HELP

Description

This parameter returns more information about a specific parameter or command.

In most cases, except special parameters, this command tells you the minimum, maximum, default, and actual value of a parameter. Exceptions are commands that do not have these values (such as DRV.EN ) or information commands (such as DRV.VER ).

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Related Topics

Terminal

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen