REC.GAP

Description

REC.GAP specifies the gap between consecutive samples. The recording base rate is 16 kHz, thus a gap of 1 means that a sample is recorded every 62.5 µs.

General Information

Type

R/W Parameter

Units

N/A

Range

1 to 65,535

Default Value

1

Data Type

Integer

See Also

REC.TRIG

Start Version

M_01-00-00-000

Related Topics

Scope

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen