VL.ERR
Description
VL.ERR sets the velocity error. It is calculated in the velocity loop as the difference between VL.CMD and VL.FB .
General Information
|
Type |
R/O Parameter |
|
Units |
Depends on UNIT.VROTARY (pg 1) or UNIT.VLINEAR (pg 1) Rotary: rpm, rps, deg/s, (custom units)/s, rad/s Linear: counts/s, mm/s, µm/s, (custom units)/s |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3407h/4 |
M_01-00-00-000 |
Related Topics
1 Velocity Loop
|
Copyright © 2018 Kollmorgen |
|