Sequential Function Chart (SFC)

The SFCClosed"Sequential function chart" It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions - Transitions with associated logic conditions - Directed links between steps and transitions language is a state diagram. Graphical steps are used to represent stable states, and transitions describe the conditions and events that lead to a change of state. Using SFC highly simplifies the programming of sequential operations as it saves a lot of variables and tests just for maintaining the program context.

Below are basic components of an SFC chart:

Chart:
 
Programming:
Steps and initial steps
Transitions and divergences
Parallel branches
Macro-steps
Jump to a step
Actions within a step
Timeout on a step
Programming a transition condition

How SFC is executed

The KAS IDEClosed"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger fully supports SFC programming with several hierarchical levels of charts: i.e. a chart that controls another chart. Working with a hierarchy of SFC charts is an easy and powerful way for managing complex sequences and saves performances at runtimeClosedIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running. Refer to the following sections for further details:

Related Topics

Sequential Function Chart (SFC) Editor

Using the SFC toolbar

SFC Editor Keyboard Shortcuts

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen