AXIS#.HOME.FEEDRATE
Description
AXIS#.HOME.FEEDRATE is the percentage of the homing speed (AXIS#.HOME.V) used when searching for the feedback’s index. AXIS#.HOME.FEEDRATE is only used in home modes 3, 6 and 10.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
|
Type |
Read/Write |
|
Units |
% |
|
Range |
1 to 100 |
|
Default Value |
50 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics