AXIS#.IL.FOLDWTHRESH
Description
AXIS#.IL"Instruction list" This is a low-level language and resembles assembly.FOLDWTHRESH is the warning level of the current foldback algorithm. When AXIS#.IL.IFOLD drops below AXIS#.IL.FOLDWTHRESH a warning is generated.
To ensure that the current foldback warning level is never reached, AXIS#.IL.FOLDWTHRESH should be set well below the continuous current value for both the drive and motor, namely AXIS#.IPEAK and AXIS#.MOTOR.IPEAK respectively. You can also set the AXIS#.IL.FOLDWTHRESH value to zero.
AXIS#.IL.FOLDWTHRESH should always be above the fault threshold AXIS#.IL.FOLDFTHRESH and below AXIS#.IPEAK and AXIS#.MOTOR.IPEAK.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Arms |
Range |
0 to 500 Arms |
Default Value |
0 A |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.IL.FOLDWTHRESH | 0x500A | 0xA | DINT | 1000:1 | - | RW | False |
AXIS2.IL.FOLDWTHRESH | 0x510A | 0xA | DINT | 1000:1 | - | RW | False |