| MLMotionInit
|
Initializes the motion library. Must be called before any other Motion Library function. Returns TRUE if the function succeeded. BasePeriod is the duration of one motion cycle in microseconds. |
BOOL |
| MLMotionRstErr
|
Re-initializes the motion engine after a motion error. Motion errors are for example communication errors of the motion bus. Returns TRUE if the function succeeded. |
BOOL |
| MLMotionStart
|
Starts the motion engine, motion bus driver, and initializes network to operational mode. Applicable to and PipesNetwork motion engines. Returns TRUE if the function succeeded. |
BOOL |
| MLMotionStatus
|
Returns the status of the motion engine
0: Not initialized
1: Running
2: Stopped
3: Error |
None |
| MLMotionStop
|
Stops the motion bus driver, motion engine, and EtherCAT network operation, resulting in the EtherCAT network transitioning to the Init state. Returns TRUE if the function succeeded. |
BOOL |
| MLMotionSysTime
|
Prints the system time to the log |
BOOL |
| MLMotionCycleTime
|
Returns the Motion Base Cycle time in seconds. |
|