Backup and Restore a PDMM or PCMM

The SD card is used for backing up and restoring the data from a AKD PDMM or PCMM.

Backing up may be performed in either of two ways.


  • For a complete backup of both the controller and drive, use the Web Server backup.

Restoring information to the controller may be performed in either of two ways. Both methods restore the controller (and PDMM drive) with whatever was saved to the SD card.

Backup & Restore What? To/From SD card via B2/B3 buttons To/From SD card via Web Server
Controller: Firmware
Controller: Network Configuration
Controller: PLC Application
Controller: Retain Variables
EtherCAT Devices: Network Topology
EtherCAT Devices: AKD Drive Firmware ‡
EtherCAT Devices: AKD Drive Parameters

‡ Restore only

About the data transfer

  • The 7-segment display will show the chasing lights animation while the backup or restore is occurring.
  • The Backup and Restore functions have an "all or nothing" behavior. If there is no SD card inserted, if there is not enough space on the card or if files are missing then nothing will be copied and the 7-segment display will show an error.
  • If files already exist on the SD card (in the backup directory), then they will be deleted and replaced with the new AKD PDMM or PCMM backup configuration files. Likewise, the files on the controller will be replaced with the SD files.

  • Warning! Do not modify the files on the SD card as this could result in the Restore function failing.


  • If you have multiple AKD PDMM or PCMM backup configurations, you will need to use one SD card per backup configuration.