AXIS#.IL.COMPTABLE.DATA
Description
AXIS#.IL
"Instruction list"
This is a low-level language and resembles assembly.COMPTABLE.DATA gets/sets the contents of the cogging compensation/torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist compensation table.
The range of the table is specified byAXIS#.IL.COMPTABLE.MIN to AXIS#.IL.COMPTABLE.MAX
When the table is enabled (AXIS#.IL.COMPTABLE.ENABLE), the output is determined by the value of AXIS#.PL.FB , the table min, max and modulo settings.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-03-000 |
General Information
|
Type |
Read/Write |
|
Units |
Amps |
|
Range |
-AXIS#.IPEAK to +AXIS#.IPEAK |
|
Index Range |
0 to 65535 |
| Default Value | 0 |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.