AXIS#.MOTOR.BRAKE
Description
The AXIS#.MOTOR.BRAKE parameter notifies the firmware whether a brake exists or not. It does not apply or release the brake. If a brake is found to be present, the firmware considers hardware indications regarding the brake circuits (such as open circuit or short circuit). If a brake does not exist, then the firmware ignores the hardware indications since they are irrelevant.
|
Value |
Status |
|---|---|
|
0 |
Motor brake does not exist. |
|
1 |
Motor brake exists and brake hardware circuitry checks are enabled. |
| 100 | For special, low current, brake applications, brake faults are bypassed with this setting. |
When the axis is enabled, setting AXIS#.MOTOR.BRAKE to 1 when no motor brake exists creates a fault.
-
-
This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET=1 and motor memory version is 0.2 or greater. This parameter can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index =1.
Examples
Context
For more information see Brake and Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0, 1, 100 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.BRAKE | 0x500B | 0x8 | USINT | - | - | RW | False |
| AXIS2.MOTOR.BRAKE | 0x510B | 0x8 | USINT | - | - | RW | False |