AXIS#.MOTOR.DISAUTOSET
-
- Advanced feature - Not recommended for general use
Description
AXIS#.MOTOR.DISAUTOSET disables autoset behavior for the parameter corresponding to the index (first argument). Under normal operation, when AXIS#.MOTOR.AUTOSET = 1 and a motor with feedback memory is selected as AXIS#.IL.FBSOURCE for the axis, the drive populates supported motor parameters automatically from the motor memory. AXIS#.MOTOR.DISAUTOSET turns this behavior off for individual parameters.
Usage
When used from the WorkBench terminal command line, AXIS#.MOTOR.DISAUTOSET may be followed by optional command line arguments. When no arguments are given, it reports the autoset disable state for all axis motor parameters (0 = autoset is not disabled, 1 = autoset is disabled).
When followed by one argument, AXIS#.MOTOR.DISAUTOSET reports the autoset disable state for a single motor parameter. The argument must be a valid integer index as defined in the table below.
When followed by two arguments, AXIS#.MOTOR.DISAUTOSET sets the autoset disable state for a motor parameter. The first argument must be a valid integer index. When the second argument is 1, autoset is turned off for the parameter. When the second argument is 0, autoset is turned back on for the parameter.
Example
The following example shows the use of AXIS#.MOTOR.DISAUTOSET for AXIS#.MOTOR.INERTIA .
--> AXIS1.MOTOR.AUTOSET 1 --> AXIS1.MOTOR.DISAUTOSET 6 0 --> DRV.HELP AXIS1.MOTOR.INERTIA Help for: AXIS1.MOTOR.INERTIA [Float] [ReadOnly] [AutoSet] Actual value = 0.200 [kg*cm^2] --> AXIS1.MOTOR.INERTIA 0.5 Error: [0007] Command is read-only. --> AXIS1.MOTOR.DISAUTOSET 6 1 --> AXIS1.MOTOR.INERTIA 0.5 --> DRV.HELP AXIS1.MOTOR.INERTIA Help for: AXIS1.MOTOR.INERTIA [Float] [NV] [ReadWrite] [AutoSet] Minval = 0.000 Maxval = 200000.000 Default = 0.000 AutoSet value = 0.200 Actual value = 0.500 [kg*cm^2] --> AXIS1.MOTOR.DISAUTOSET 6 0 --> DRV.HELP AXIS1.MOTOR.INERTIA Help for: AXIS1.MOTOR.INERTIA [Float] [ReadOnly] [AutoSet] Actual value = 0.200 [kg*cm^2]
Context
For more information see Motor
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0, 1 |
|
Default Value |
0 |
|
Data Type |
Array |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.