AXIS#.PL.AINSOURCE
Description
This parameter sets which analog input to use for AXIS#.PL.AINSCALE.
Value | Description |
---|---|
0 | Uses no analog input. The position command in analog position mode is equal to the position feedback. |
1 | Uses AIN1 |
2 | Uses AIN2 |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 | |
Added '0' to range | 02-07-02-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 2 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.