AXIS#.SM.DEC

Description

Sets the deceleration ramp for service motion if set to greater than 0.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPMClosed "Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Units for details.

Default Value

30,000 rpm/s

Depends on units. See Acceleration Units for details.

Data Type

Float

See Also

Service Motion

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported