AXIS#.DBILIMITACTUAL
Description
This parameter returns the minimum value of the following parameters: AXIS#.DBILIMIT , AXIS#.ICONT , AXIS#.MOTOR.ICONT .
Example
Assume AXIS1.ICONT = 3 Arms, AXIS1.DBILIMIT = 1 Arms, and AXIS1.MOTOR.ICONT = 2 Arms. Then AXIS#.DBILIMITACTUAL will return 1 Arms.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-00-000 |
General Information
|
Type |
Read only |
|
Description |
Returns the minimum value of the AXIS#.DBILIMIT , AXIS#.ICONT , AXIS#.MOTOR.ICONT keywords. |
|
Units |
Arms |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.DBILIMITACTUAL | 0x5000 | 0x11 | UDINT | 1000:1 | - | RO | False |
| AXIS2.DBILIMITACTUAL | 0x5100 | 0x11 | UDINT | 1000:1 | - | RO | False |