AXIS#.SETUPREQBITS
Description
AXIS#.SETUPREQBITS is a bit-field that returns the set of parameters that needs to be set up before the drive can be enabled. The drive can only be enabled when this parameter returns 0.
-
-
If AXIS#.MOTOR.AUTOSET is set to 1 (parameters automatically calculated from motor ID data), then all values in the list will be initialized from the feedback device
A process whereby some proportion of the output signal of a system is passed (fed back) to the input.
In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position. Otherwise, the parameters must be set manually.
The following table lists the parameters which require setup for each motor type.
| Index | Bit | Default Value | Induction Motor V/f Open Loop |
Induction Motor Closed Loop |
Interior Permanent Magnet |
|---|---|---|---|---|---|
| AXIS#.IL |
0 | 50 [V/A] | - | √ | √ |
| AXIS#.MOTOR.IPEAK | 1 | 2 Arms | √ | √ | √ |
| AXIS#.MOTOR.ICONT | 2 | 1 Arms | √ | √ | √ |
| AXIS#.MOTOR.POLES | 4 | 6 | √ | √ | √ |
| AXIS#.MOTOR.LQLL | 7 | 17mH | - | - | √ |
| AXIS#.MOTOR.LDLL | 8 | 17mH | - | - | √ |
| AXIS#.MOTOR.KE | 9 | 0 | - | - | √ |
| AXIS#.MOTOR.IMTR | 10 | 100ms | - | √ | - |
| AXIS#.MOTOR.IMID | 11 | 0 | - | √ | - |
| AXIS#.MOTOR.VOLTRATED | 12 | 230 Vrms |
√ | - | - |
| AXIS#.MOTOR.VRATED | 13 | 0 | - | - | √ |
| AXIS#.MOTOR.LISAT | 14 | 25 x DRIVE.IPEAK | - | - | √ |
| AXIS#.MOTOR.VRIDK1 | 15 | 0 | - | - | √ |
| AXIS#.MOTOR.VRIDK2 | 16 | 0 | - | - | √ |
| AXIS#.MOTOR.IDMAX | 17 | 0.5 x AXIS#.MOTOR.IPEAK | - | - | √ |
| AXIS#.IL.KDPRATIO | 18 | 1 | - | - | √ |
| AXIS#.MOTOR.PITCH | 19 | 32 | - | - | - |
| AXIS#.MOTOR.VOLTMAX | 20 | 480 Vrms | - | - | √ |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer (bit-field) |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics