CAP#.EDGE

Description

Selects which edge of the trigger input to use.

The trigger source is monitored for either a rising, falling, or either edge. When one of these edges is detected the position or time is captured. This setting is always used irrespective of the precondition configuration.

Examples

Usage

1: Rising edge (default)

2: Falling edge

3: Rising or falling edge

Code

-->CAP1.EDGE 1
-->

Context

For more information please refer to Capture.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 3

Default Value

1

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Related Topics

Capture

CAP#.PREEDGE