CAP#.PREEDGE
Description
If precondition mode 1 has been selected, then this selects which edge of the precondition input will be waited for before the trigger is allowed.
Examples
Usage
1: Rising edge (default)
2: Falling edge
3: Rising or falling edge
Code
-->CAP1.EDGE 1 -->
Context
For more information please refer to Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 3 |
|
Default Value |
1 |
|
Data Type |
Integer |
| See Also | CAP#.PREMODE, CAP#.PRESELECT |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics
Capture