CAP#.PRESELECT
Description
Selects the digital input used as the precondition input.
Examples
Usage
| Value | Description |
|---|---|
|
1-12 (2 is the default) |
Digital Inputs DIN1 to 12 |
|
21 – 26
|
Bidirectional digital inputs. DIO1 to 6 |
|
31 – 35 |
Z-Pulses from feedbacks 1 to 5 |
|
41 - 42 |
Z-pulse from Axis 1 or 2 |
Not all hardware variants have the hardware to support all of these options. For example, a single axis drive will not support option 42.
Code
-->CAP1.PRESELECT 21 -->
Context
For more information please refer to Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 12, 21 to 26, 31 to 35, 41 to 42 |
|
Default Value |
2 |
|
Data Type |
Integer |
| See Also | CAP#.PREMODE, CAP#.PREEDGE |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics
Capture