CAP#.TRIGGER

Description

Selects which input will trigger the capture.

Examples

Usage

Value Description
1-12 where 1 (default) Digital Inputs DIN1 to 12
21-26 Bidirectional digital inputs. DIO1 to 6
31-35 Z-Pulses from feedbacks FB1 to 5
41-42 Z-pulse from Axis 1 or 2

Not all drive models have the hardware to support all these options. For example, a single axis drive can not support 42.

Code

-->CAP1.TRIGGER 41

-->

Context

For more information please refer to Capture.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 12, 21 to 26, 31 to 35, 41 to 42

Default Value

1

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Related Topics

Capture

CAP#.PRESELECT