FB#.PRINTMOTORDATA
Description
FB#.PRINTMOTORDATA reads the contents of the motor data file stored in feedback memory if the feedback device
A process whereby some proportion of the output signal of a system is passed (fed back) to the input.
In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position supports motor memory.
Context
See Feedback Settings.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.