FB#.RESREFPHASE
Description
This parameter sets the electrical degrees of phase lag in the resolver.
See the motor resolver datasheet for the value for this parameter.
Context
See Feedback Settings.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
electrical degrees |
|
Range |
-180 to 180° |
|
Default Value |
-2° |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
FB1.RESREFPHASE | 0x3500 | 0x5 | UDINT | - | - | RW | False |
| FB2.RESREFPHASE | 0x3501 | 0x5 | UDINT | - | - | RW | False | |
| FB3.RESREFPHASE | 0x3502 | 0x5 | UDINT | - | - | RW | False | |
| FB4.RESREFPHASE | 0x3503 | 0x5 | UDINT | - | - | RW | False | |
| FB5.RESREFPHASE | 0x3504 | 0x5 | UDINT | - | - | RW | False |