DRV.FAULT1 to DRV.FAULT10

Description

These parameters are holding registers where any active faults will be kept. A value of zero represents that no fault is present. Non-zero values correspond to specific fault codes in the drive (see fault and warning messages). The registers are populated in the order of when the fault occurs (DRV.FAULT1, DRV.FAULT2, DRV.FAULT3, and so on).

Notes:

  • DRV.FAULT1 to DRV.FAULT10 are only updated when DRV.FAULT1 is read. If the fault does not exist when DRV.FAULT1 is read, it may not be registered in DRV.FAULT2 to DRV.FAULT10.
  • If DRV.FAULT1 value is 0, then the drive does not have any faults.
  • Only active faults are shown. This is not a fault history.
  • These registers are an alternative to the string type parameter DRV.FAULTS, so that fieldbusses and AKD BASIC users have easier access to the details of the faults in the drive.
  • Warnings are not shown in the registers, only faults.

General Information

Type

R/O

Units

N/A

Range

Any supported fault code or 0.

Default Value

N/A

Data Type

Integer

Start Version

M_01-06-00-000

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

2001h/1

DRV.FAULT1

M_01-00-00-000

2001h/2

DRV.FAULT2

2001h/3

DRV.FAULT3

2001h/4

DRV.FAULT4

2001h/5

DRV.FAULT5

2001h/6

DRV.FAULT6

2001h/7

DRV.FAULT7

2001h/8

DRV.FAULT8

2001h/9

DRV.FAULT9

2001h/A

DRV.FAULT10

Related Topics

DRV.ACTIVE | DRV.WARNING1 to DRV.WARNING3