DRV.WARNING1 to DRV.WARNING3

Description

These parameters are holding registers where any active warnings will be displayed. A value of zero represents that no warning is present. Non-zero values correspond to specific warning codes in the drive (see fault and warning messages). The registers are populated in the order of when the warning occurs (DRV.WARNING1, DRV.WARNING2, DRV.WARNING3, and so on).

Notes:

General Information

Type

R/O

Units

N/A

Range

Any supported fault code or 0

Default Value

N/A

Data Type

Integer

Start Version

 

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

2000h/1

DRV.WARNING1

M_01-00-00-000

2000h/2

DRV.WARNING2

2000h/3

DRV.WARNING3

Related Topics

DRV.FAULT1 to DRV.FAULT10 |