CASE OF ELSE END_CASE
Syntax
CASE <DINT expression> OF
<value> :
<statements>
<value> , <value> :
<statements>;
<value> .. <value> :
<statements>;
ELSE
<statements>
END_CASE;
Remarks
- All enumerated values correspond to the evaluation of the DINT expression and are possible cases in the execution of the statements.
- The statements specified after the ELSE keyword are executed if the expression takes a value which is not enumerated in the switch.
- For each case, you must specify either:
- a value.
- a list of possible values separated by comas (,).
- a range of values specified by a "min .. max" interval.
- You must enter space characters before and after the ".." separator.
FBD Language
Not available.
FFLD Language
Not available.
IL Language
Not available.
ST Language
(* This example check first prime numbers: *)
CASE iNumber OF
0 :
Alarm := TRUE;
AlarmText := '0 gives no result';
1 .. 3, 5 :
bPrime := TRUE;
4, 6 :
bPrime := FALSE;
ELSE
Alarm := TRUE;
AlarmText := 'I don't know after 6 !';
END_CASE;
See Also