FOR TO BY END_FOR
Syntax
FOR <index> := <minimum> TO <maximum> BY <step> DO
<statements>
END_FOR;
index = DINT internal variable used as index.
minimum = DINT expression: initial value for index.
maximum = DINT expression: maximum allowed value for index.
step = DINT expression: increasing step of index after each iteration (default is 1) .
Remarks
- The BY <step> statement can be omitted.
- The default value for the step is 1.
FBD Language
Not available.
FFLD Language
Not available.
IL Language
Not available.
ST Language
iArrayDim := 10;
(* resets all items of the array to 0 *)
FOR iPos := 0 TO (iArrayDim - 1) DO
MyArray[iPos] := 0;
END_FOR;
(* set all items with odd index to 1 *)
FOR iPos := 1 TO 9 BY 2 DO
MyArray[ipos] := 1;
END_FOR;
See Also