EXIT
Remarks
- The EXIT statement indicates that the current loop (FOR, REPEAT, or WHILE) must be finished.
- The execution continues after the END_FOR, END_REPEAT, or END_WHILE keyword or the loop where the EXIT is.
- EXIT quits only one loop and cannot be used to exit at the same time several levels of nested loops.
-
-
Loop instructions can lead to infinite loops that block the target cycle.
FBD Language
Not available.
FFLD Language
Not available.
IL Language
Not available.
ST Language
(* This program searches for the first non null item of an array: *)
iFound = -1; (* means: not found *)
FOR iPos := 0 TO (iArrayDim - 1) DO
IF iPos <> 0 THEN
iFound := iPos;
EXIT;
END_IF;
END_FOR;
See Also