Instruction List (IL)
A program written in IL
"Instruction list"
This is a low-level language and resembles assembly language is a list of instructions.
- Each instruction is written on one line of text.
- An instruction can have one or more operands.
- Operands are variables or constant expressions.
- Each instruction can begin with a label, followed by the ":" character.
- Labels are used as destination for jump instructions.
The KAS IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger allows
you to mix ST
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal and IL languages in textual program. ST is the default
language. When you enter IL instructions, the program must be entered
between "BEGIN_IL" and "END_IL" keywords, such as in the following example:
BEGIN_IL
FFLD var1
ST var2
END_IL
Comments
Comment texts can be entered at the end of a line containing an instruction. Comment texts have no meaning for the execution of the program. A comment text must begin with "(*" and end with "*)". Comments can also be entered on empty lines (with no instruction), and on several lines (i.e. a comment text can include line breaks). Comment texts cannot be nested.
(* My comment *)
LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them a
ST b (* Store value in d *)
Data flow
An IL complete statement is made of instructions for:
- first: evaluating an expression (called current result)
- then: use the current result for performing actions
Evaluation of expressions
The order of instructions in the program is the one used for evaluating expressions, unless parentheses are inserted. Below are the available instructions for evaluation of expressions:
|
Instruction |
Operand |
Meaning |
| FFLD / FFLDN | any type | Loads the operand in the current result. |
| AND (&) | Boolean | AND between the operand and the current result. |
| OR / ORN | Boolean | OR between the operand and the current result. |
| XOR / XORN | Boolean | XOR between the operand and the current result. |
| ADD | numerical | Adds the operand and the current result. |
| SUB | numerical | Subtract the operand from the current result. |
| MUL | numerical | Multiply the operand and the current result. |
| DIV | numerical | Divide the current result by the operand. |
| GT | numerical | Compares the current result with the operand. |
| GE | numerical | Compares the current result with the operand. |
| LT | numerical | Compares the current result with the operand. |
| LE | numerical | Compares the current result with the operand. |
| EQ | numerical | Compares the current result with the operand. |
| NE | numerical | Compares the current result with the operand. |
| Function call | func. arguments | Calls a function. |
| Parenthesis | Changes the execution order. |
-
-
Instructions suffixed by N uses the Boolean negation of the operand.
Actions
The following instructions perform actions according to the value of current result. Some of these instructions do not need a current result to be evaluated:
|
Instruction |
Operand |
Meaning |
| ST / STN | any type | Stores the current result in the operand. |
| JMP | label | Jump to a label - no current result needed. |
| JMPC | label | Jump to a label if the current result is TRUE. |
| JMPNC / JMPCN | label | Jump to a label if the current result is FALSE. |
| RET | Jump to the end of the current program - no current result needed. | |
| RETC / RETNC / RETCN | Jump to the end of the current program if the current result is TRUE / FALSE. | |
| S | Boolean | Sets the operand to TRUE if the current result is TRUE. |
| R | Boolean | Sets the operand to FALSE if the current result is TRUE. |
| CAL | f. block | Calls a function block (no current result needed). |
| CALC | f. block | Calls a function block if the current result is TRUE. |
| CALNC / CALCN | f. block | Calls a function block if the current result is FALSE. |
-
-
Instructions suffixed by N uses the Boolean negation of the operand.
-
-
IL program cannot be called if there is no entry variable, or if its type is complex (e.g. array).