MCFB_StepAbsSwitchFastInput
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Fast homing to a home switch.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
0, 1 |
N/A |
No default |
Request the homing step procedure at the rising edge Outputs are reset when execute input is FALSE. |
|
AxisID |
AXIS_REF |
1, 256 |
N/A |
No default |
Structure for specified Axis designated to home. See AXIS_REF Structure for more information. |
|
Direction |
BOOL |
0, 1 |
N/A |
No default |
Defines the axis homing direction.
|
|
SwitchMode |
DINT |
0, 3 |
N/A |
No default |
Switch state to complete homing.
|
|
Velocity |
LREAL |
No range |
User unit/sec |
No default |
Commanded velocity for the homing move. |
|
Acceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Commanded acceleration for the homing move. |
|
Deceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Commanded deceleration for the homing move. |
|
LREAL |
No range |
User unit/sec3 |
No default |
Commanded jerk If 0 (zero), trapezoidal acc/dec is used. |
|
|
TorqueLimit |
LREAL |
No range |
User units |
No default |
Maximum torque
|
|
TimeLimit |
TIME |
No range |
Sec |
No default |
Maximum time for homing move to complete.
|
|
DistanceLimit |
LREAL |
No range |
User units |
No default |
Maximum distance for homing move to complete.
|
|
FastInputNum |
BOOL |
0, 1 |
N/A |
No default |
|
|
PosLimitSwitch |
BOOL |
0, 1 |
N/A |
No default |
The positive direction limit switch input I/O point. |
|
NegLimitSwitch |
BOOL |
0, 1 |
N/A |
No default |
The negative direction limit switch input I/O point. |
|
BufferMode |
SINT |
0, 5 |
N/A |
No default |
Define the homing move start action.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Done |
BOOL |
|
N/A |
Indicates the move completed successfully. |
||||||||||||||
|
Busy |
BOOL |
|
N/A |
High from the moment the Execute input goes high until the time the move is ended. |
||||||||||||||
|
Active |
BOOL |
|
N/A |
Set when the function block is active. |
||||||||||||||
|
CommandAborted |
BOOL |
|
N/A |
Indicates the move was aborted. |
||||||||||||||
|
Error |
BOOL |
|
N/A |
Signals an error has occurred within the function block. |
||||||||||||||
|
ErrorID |
INT |
|
N/A |
Indicates the error if the Error output is set to TRUE. Error identifier:
|
||||||||||||||
|
TriggerPosition |
LREAL |
No range |
User units |
|
Remarks
- Performs a homing function by searching for an absolute positioned external physical switch.
- An Absolute Switch has two Off (or On) areas.
This image shows the function or function block I/O.
Figure 6-96: MCFB StepAbsSwitchFastInput
Usage
- The homing is commanded in the most likely direction where the sensor can be found.
- If any LimitSwitch is found during Homing
The Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position (any of them), a special process is started in the opposite direction. - The AbsSwitch is searched to switch Off (or On, depending on SwitchMode setting).
- The Edge (passed by) and homing process is restarted in the original direction and with the same conditions.
- This ensures the end conditions are always the same.
FBD Language Example
FFLD Language Example
PosLimitSwitch, NegLimitSwitch are declared I/O points.
IL Language Example
Not available.
ST Language Example
Execute_1 :=1;
(*Positive_Switch and Negitive_Switch are physical hardware in Dictionary. *)
Inst_MC_StepAbsSwitchFastInput( Execute_1, Axis1, 0, 0, 10000.0,Acceleration:=10000.0, 10000.0, 0, 0, 0, 0, 0, Positive_Switch , Negitive_Switch , 0)
HomeComplete := Inst_MC_StepAbsSwitchFastInput.Done;
HomeBusy := Inst_MC_StepAbsSwitchFastInput.Busy;
HomeActive := Inst_MC_StepAbsSwitchFastInput.Active;
HomeAborted := Inst_MC_StepAbsSwitchFastInput.CommandAborted;
HomeError := Inst_MC_StepAbsSwitchFastInput.Error;
HomeErrorID := Inst_MC_StepAbsSwitchFastInput.ErrorID;
HomeTriggerPosition := Inst_MC_StepAbsSwitchFastInput.TriggerPosition;
See Also