MLFB_HomeFindHomeFastInputModulo
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Fast homing to a home switch: Modulo mode.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ibExecute |
BOOL |
0, 1 |
N/A |
No default |
Request the homing step procedure at the rising edge |
|
iAxisID |
AXIS_REF |
1, 256 |
N/A |
No default |
Name of a declared instance of the AXIS_REF library function. See AXIS_REF Structure for more information. |
|
iPosition |
LREAL |
No range |
User units |
No default |
Offset position applied after home switch is found. |
|
ibDirection |
BOOL |
0, 1 |
N/A |
No default |
Defines the axis homing direction.
|
|
iVelocity |
LREAL |
No range |
User unit/sec |
No default |
Commanded velocity for the homing move. |
|
iAcceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Commanded acceleration for the homing move. |
|
iDeceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Commanded deceleration for the homing move. |
|
ibLimitSwitchMode |
BOOL |
0, 1 |
N/A |
No default |
Limit switch state to complete homing.
|
|
ibPosLimitSwitch |
BOOL |
0, 1 |
N/A |
No default |
The positive direction limit switch input I/O point. |
|
ibNegLimitSwitch |
BOOL |
0, 1 |
N/A |
No default |
The negative direction limit switch input I/O point. |
|
iTimeout |
TIME |
No range |
Sec |
No default |
Maximum time for homing move to complete.
|
|
ibFastInputNumber |
BOOL |
0, 1 |
N/A |
No default |
Limit switch state to complete homing. |
|
iCycleTime |
LREAL |
No range |
Microseconds |
No default |
Either 250, 500, or 1000. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
obDone |
BOOL |
|
N/A |
Indicates the move completed successfully. |
||||||||||||
|
obActive |
BOOL |
|
N/A |
Indicates this move is the Active move. |
||||||||||||
|
obError |
BOOL |
|
N/A |
Indicates either:
|
||||||||||||
|
oErrorID |
DINT |
|
N/A |
Indicates the error if the Error output is set to TRUE. Error identifier:
|
Remarks
- Performs a single-axis home to a limit switch connected to a High Speed Input.
- This function is used when the axis is set-up in Modulo mode.
- The motor starts to move according to the direction setting.
- The home position has been found as soon as the fast input
The inputs are taken into account at each cycle depending on the system periodicity (for example each millisecond). Under certain circumstances this can be insufficient when more accuracy is needed, or if a quick response is required from the system. To fill the gap, a drive may have some Fast Input connections (generally one or two). When an event happens that triggers a Fast Input (e.g. when a sensor sends a rising edge), the detection of a signal occurs faster (which can be 1000 times more accurate than the system periodicity). Then the timestamp associated with this input can be provided to the IPC to take corrective action selected is triggered on the edge selected.
- The home position has been found as soon as the fast input
- An absolute move is made to the triggered position and the position value is set.
- The hardware limit switches are monitored during the homing procedure.
- The drive behaves this way in case a hardware limit switch is active before the home-switch has been activated:
The motor changes the direction until the home switch is crossed.
This image shows the function or function block I/O.
Figure 6-87: MLFB HomeFindHomeFastInputModulo
Usage
- This procedure performs a homing function searching for a sensor
A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer using only High Speed Input Switches. - A High Speed Limit Switch has 1 Off (or On) area.
- Home is commanded by the user in the designated homing direction at the selected or programmed Velocity.
- If LimitSwitch is found On with a rising Execute, the process is started in the opposite direction as specified.
- If LimitSwitch is found Off Edge (released), the process is restarted again in original direction.
This can be On, depending on LimitSwitchMode setting.- This ensures the end conditions are always the same.
- The Timeout can cause an error if exceeded.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Direction:= 0;
Position:=1000;
Velocity:=1000;
Acceleration:=10000;
Deceleration:=10000;
SwitchMode:=0;
Timeout:=T#100;
FastInputNumber:=0;
CycleTime:=1000;
inst_fbHomeFindHomeFastInputModulo(True, Axis1, Position, Direction, Velocity, Acceleration, Deceleration, PosLimitSwitch, NegLimitSwitch, Timeout, FastInputNumber, CycleTime);
HomeComplete :=inst_fbHomeFindHomeFastInputModulo.Done;
HomeActive :=inst_fbHomeFindHomeFastInputModulo.Active;
HomeError :=inst_fbHomeFindHomeFastInputModulo.Error;
HomeErrorID :=inst_fbHomeFindHomeFastInputModulo.ErrorID;
(* PosLimitSwitch and NegLimitSwtch are declared I/O points *)
See Also