MLFB_HomeFindLimitInput
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Homing
The Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position to a limit switch.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ibExecute |
BOOL |
|
|
|
Start homing, edge-triggered. |
|
iAxisID |
DINT |
|
|
|
ID of the axis block of the Pipe Network. |
|
iPosition |
LREAL |
|
|
|
Reference position. |
|
ibDirection |
BOOL |
|
|
|
|
|
iVelocity |
LREAL |
|
|
|
Reference speed. |
|
iAcceleration |
LREAL |
|
|
|
Reference acceleration. |
|
iDeceleration |
LREAL |
|
|
|
Reference deceleration. |
|
ibLimitSwitch |
BOOL |
|
|
|
Positive or negative limit switch, high-active. Depends on the ibDirection. |
|
iTimeout |
TIME |
|
|
|
Time monitoring (T#0ms: off). |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
obDone |
BOOL |
|
|
Done bit. |
||||||||||||
|
obActive |
BOOL |
|
|
Active bit. |
||||||||||||
|
obError |
BOOL |
|
|
Error bit. |
||||||||||||
|
oErrorID |
DINT |
|
|
Error identifier:
|
Remarks
- The find limit input mode moves to a limit input.
- This method is used if you have a positive or negative limit switch available that you want to establish as a home reference point.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Call homing function on Axis1 with preset velocity, accel, and decel values
//Start in negative direction and stop when axis hits limit switch or times out
//after seeing limit switch, set axis position to zero
Inst_MLFB_HomeFindLimitInput( StartHomeRoutine,
PipeNetwork.AXIS1,
0,
TRUE,
100,
1000,
1000,
HomeDigitalInput,
T#30s );
HomeDone := Inst_MLFB_HomeFindLimitInput.obDone;
See Also