MLFB_HomeMoveUntilPosErrExceeded
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Homing
The Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position to the position error is exceeded.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ibExecute |
BOOL |
|
|
|
Start homing, edge-triggered. |
|
iAxisID |
DINT |
|
|
|
ID of the axis block of the Pipe Network. |
|
iPosition |
LREAL |
|
|
|
Reference position. |
|
ibDirection |
BOOL |
|
|
|
|
|
iVelocity |
LREAL |
|
|
|
Reference speed. |
|
iAcceleration |
LREAL |
|
|
|
Reference acceleration. |
|
iDeceleration |
LREAL |
|
|
|
Reference deceleration. |
|
iMaxPositionError |
LREAL |
|
|
|
Maximum position error. |
|
iPeakCurrent |
DINT |
|
|
|
Peak current in mA. |
|
iTimeout |
TIME |
|
|
|
Time monitoring (T#0ms: off). |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
obDone |
BOOL |
|
|
Done bit. |
||||||||||||
|
obActive |
BOOL |
|
|
Active bit. |
||||||||||||
|
obError |
BOOL |
|
|
Error bit. |
||||||||||||
|
oErrorID |
DINT |
|
|
Error identifier:
|
Remarks
- When executed, the motor will move to the hard stop with a definable peak current.
- When the position error exceeds, the home Position is set.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Call homing function on Axis1 with preset velocity, accel, and decel values
//Start in negative direction and go until position error exceeds input value or time out
//afterterwards set axis position to zero
//function block temporarily writes new max current value to 2 Amp while home routine active
Inst_MLFB_HomeMoveUntilPosErrExceeded( StartHomeRoutine,
PipeNetwork.AXIS1,
0,
1,
100,
1000,
1000,
MaxPosError,
2000,
T#30s );
HomeDone := Inst_MLFB_HomeMoveUntilPosErrExceeded.obDone;
See Also