MC_InitAxesGrp
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Initializes the kinematic limits for the axis group.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
0, 1 |
N/A |
No default |
On the rising edge |
|
AxesGroup |
No range |
N/A |
No default |
The axes group to be initialized. |
|
|
VelocityLimit |
LREAL |
0 < Velocity < (20 * Acceleration) and 0 < Velocity < (20 * Deceleration) 0 < Velocity < (20 * Acceleration) and |
User unit/sec |
No default |
Velocity limit. See Limitations on Acceleration and Jerk for more information. |
|
AccelerationLimit |
LREAL |
0 < Velocity < (20 * Acceleration) |
User unit/sec2 |
No default |
Acceleration limit. See Limitations on Acceleration and Jerk for more information. |
|
DecelerationLimit |
LREAL |
0 < Velocity < (20 * Deceleration) |
User unit/sec2 |
No default |
Deceleration limit. See Limitations on Acceleration and Jerk for more information. |
|
JerkLimit |
LREAL |
(Velocity / 20) < Acceleration < (2 * Jerk) and (Velocity / 20) < Deceleration < (2 * Jerk) |
User unit/sec2 |
No default |
Jerk limit. See Limitations on Acceleration and Jerk for more information. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
No range |
N/A |
If TRUE, the command completed successfully. |
|
Error |
BOOL |
No range |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
No range |
N/A |
Indicates the error if Error output is TRUE. See the table in PLCopen Function Block ErrorIDs. |
Remarks
-
-
The function block returns an error if the group state is not GroupStandby or GroupDisabled.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- During a move, the motion engine verifies that the limits are not exceeded.
Figure 6-126: MC_InitAxesGrp
FBD Language Example
FFLD Language Example
IL Language Example
BEGIN_IL"Instruction List" This is a low-level language and resembles assembly CAL Inst_MC_InitAxesGrp( initAxesGrp, grp, velLim, accelLim, decelLim, jerkLim )
END_IL
ST Language Example
(* Inst_MC_InitAxesGrpST example *)Inst_MC_InitAxesGrp( initAxesGrp, grp, velLim, accelLim, decelLim, jerkLim );
See Also