MC_ReadActVel
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Reads the actual velocity of the axis.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Enable |
BOOL |
0, 1 |
N/A |
No default |
Request to read the axis's actual velocity. |
|
Axis |
AXIS_REF |
1, 256 |
N/A |
No default |
Name of a declared instance of the AXIS_REF library function.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Valid |
BOOL |
|
|
Indicates the value at the ActualVelocity output is available. |
|
Busy |
BOOL |
|
|
Indicates this function block is executing. |
|
Error |
BOOL |
|
|
Indicates an invalid input was specified. |
|
ErrorID |
INT |
|
|
Indicates the error if Error output is TRUE. See PLCopen Function Block ErrorIDs for more information. |
|
ActualVelocity |
LREAL |
|
User unit/sec |
Oscillations may be seen because this is an instant velocity, not an average velocity. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller for more information.
See Function Blocks - General Rules for more information about how inputs and outputs work.
Figure 6-215: MC_ReadActVel
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
* MC_ReadActVel S
T example *);
Inst_MC_ReadActVel( TRUE, Axis1 ); //Inst_MC_ReadActVel is an instance of MC_ReadActVel function block
ActualVel := Inst_MC_ReadActVel.ActualVelocity; // store ActualVelocity output into a user defined variable