MC_MarkRegist
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Enables Mark-to-Mark registration.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
En |
BOOL |
0, 1 |
N/A |
No default |
On the rising edge |
|
Axis |
AXIS_REF |
The range of .AXIS_NUM is [1, 256] |
N/A |
N/A |
Axis to apply registration to. |
|
TriggerInput |
TRIGGER_REF |
No range |
N/A |
No default |
The structure elements are: DirectionINT Range = 1, 5.
InputID INT Range = 0, 1
TrigIDINT Range = 0, 256.
|
|
Distance |
LREAL |
When converted to feedback units, the range is [-251, 251-1]. |
User units |
N/A |
|
|
Tolerance |
LREAL |
When converted to feedback units, |
User units |
N/A |
This value specifies the distance, plus or minus, about Distance to determine if the mark detected by the fast input is a good mark. |
|
Ignore |
LREAL |
|
User units |
N/A |
|
|
Target |
LREAL |
When converted to feedback units, the range is [-251, 251-1]. |
User units |
N/A |
|
|
Position |
LREAL |
When converted to feedback units,
|
User units |
N/A |
|
|
Options |
UINT |
See the MC_MachRegist Options Table. |
N/A |
N/A |
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
RegistOn |
BOOL |
No range |
N/A |
Indicates registration is activated. |
|
Aborted |
BOOL |
No range |
N/A |
Indicates registration has been terminated by MC_StopRegist. |
|
Error |
BOOL |
No range |
N/A |
Indicates an invalid input was specified or the registration was terminated due to an error. |
|
ErrorID |
INT |
No range |
N/A |
|
Remarks
-
- This function block starts a motion-related action and stores data for calculations and error checking.
See Call Function Blocks Multiple Times in the Same Cycle if using a dual-core controller.
-
- Is this the right function block to use?
See Decide which Function Blocks to Use for Registration and Registration Application Guide.
- It is used on any servo or digitizing axis and with any move type.
- It is used most frequently in master/slave applications.
|
Used with ... |
Effect |
|---|---|
|
Non-slave moves |
Resets the axis position when a good mark is captured by the fast input. |
|
Slave moves |
In addition to resetting the axis position, applies a compensation offset to correct for the difference between the target mark-to-mark distance and the measured mark-to-mark distance. This provides the ability to compensate for product or process inconsistencies, provides a system that remains synchronized with no accumulated error, and maintains repeatable accuracy throughout the process. |
Transition and Registration
- A positive transition of the En input starts registration.
- The application may change the registration parameters while registration is active by changing the input values and causing another positive transition of the En input.
- The function block then reads and applies the new values.
- The axis number at the Axis input identifies the axis of registration.
- If Axis is a master axis for another axis’s slave move, Master Registration is activated.
- Master Registration calculates a compensation that is added to the master offset of its slaves.
- This offset shifts the position of the master axis as seen by its slaves.
- The compensation is not applied to the master axis, but to its slaves.
- If Axis is a slave axis, Slave Registration is activated.
- Slave Registration calculates a compensation that is added to the slave offset of the axis.
- This compensation value is applied directly to the slave axis.
Distance, Tolerance, and Ignore Inputs
- The Distance, Tolerance, and Ignore inputs are used to determine whether or not the registration mark is good.
- For a mark to be recognized as good, it must be outside of the Ignore distance and the correct Distance from the previous mark +/- the Tolerance window.
- A mark is bad if it occurs outside of the “good tolerance band” and is not ignored.
- Both good marks and bad marks are recognized as marks, ignored marks are not recognized.
- If all marks are to be recognized as good marks, enter 0 (zero) at both Distance and Tolerance.
- The Distance value defines the distance between good marks.
- In Clear Lane and Product registration the Distance input value is typically the same as the Target input value.
- In Print registration, the Distance is typically not the same as Target.
- The Tolerance value is the distance, plus and minus, about Distance.
- Marks detected in this window are good marks and registration occurs.
- Marks detected outside this window and outside the Ignore band, are bad marks and registration does not occur.
- This window should be large enough to allow for the worst case error in the distance between the previous mark and the current mark.
- The Ignore value defines the distance from the previous mark where all marks detected by the fast input are ignored.
- This is crucial when registering products that do not have Clear Lane registration marks.
Target Input
- The Target input is the expected distance between good registration marks.
- It is used to calculate how much registration compensation is applied when a registration mark is considered good.
- In many applications, this is equivalent to the product length or the cycle length.
- When a good mark is detected, the actual distance between the good mark and the previous mark is determined and compared to the Target distance to calculate a correction.
- The registration correction is only applied with master/slave move types and always affects the slave axis.
Position and Option Inputs
- The Position input is the position value the registration Axis position is reset to when a good registration mark is detected.
- The Option input defines various modes of operation for registration.
- The first bit, 0001H, selects Absolute or Resetting.
- This refers to the way the second mark and all subsequent marks are determined to be good marks.
- With both registration schemes, the very first detected mark is the starting point.
- With Resetting registration, when the next mark is detected, the position of that mark becomes the starting point for the next good mark detection calculation and so on.
- The starting point is reset with each good or bad mark.
- This allows the product to re-synchronize, if necessary, due to process issues (e.g., product shift) etc.
- Absolute registration determines all good marks based on the very first mark.
- The position of the second and each subsequent mark is compared to an integer multiple of Distance from the very first mark.
- This method insures the product always registers to a known fixed distance.
Figure 6-259: MC_MarkRegist
MC_MachRegist Options Table
|
Hexadecimal |
Decimal |
Option |
Description |
|---|---|---|---|
|
0001 H |
1 |
Absolute/Resetting |
0 = Resetting, 1 = Absolute |
|
0002 H |
2 |
Reserved |
0 |
|
0004 H |
4 |
Time/position based capture |
0 = time based capture, 1 = position based capture |
|
0008 H |
8 |
Inhibit Reference on Good Mark |
0 = Perform reference, 1 = inhibit reference When this bit is set, the Position function block argument is unused and the axis position is not changed when a registration mark is encountered. |
|
0010H |
16 |
Inhibit Master Compensation |
0 = Perform Master Compensation, 1 = Inhibit Master Compensation |
|
0020H |
32 |
Inhibit Slave Compensation |
0 = Perform Slave Compensation, 1 = Inhibit Slave Compensation. |
-
-
To use Capture Engine 1, modify the input PDOs that are used and add the Latch
The control word is used to activate the drive's latch status machine. The latch control word is processed independently of the EtherCAT bus cycle. The status word is used to return the drive's latch status Position 1 parameter.
FBD Language Example
FFLD Language Example
IL Language Example
CAL Inst_MC_MarkRegist( ActivateReg, Axist1, Trig1, 360, 5, 90, 360, 0 0 )
ST Language Example
Inst_MC_MarkRegist( ActivateReg, Axist1, Trig1, 360, 5, 90, 360, 0, 0 );
See Also