MLAxisInit
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Initializes an axis object.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Acceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Sets the Axis Acceleration value. See Set the Axis Block Position Units for more information. |
|
AxisID |
DINT |
No range |
N/A |
No default |
ID Name of the Axis block. |
|
Deceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Sets the Axis Deceleration value. See Set the Axis Block Position Units for more information. |
|
FeedbackUnitPerTurn |
DINT |
No range |
User units |
No default |
|
|
InitialPosition |
LREAL |
No range |
User units |
No default |
Initial position value expressed in user logical units.
|
|
Modulo |
BOOL |
0, 1 |
N/A |
No default |
Define the mode which can be Modulo (True) or not (False). |
|
ModuloPosition |
LREAL |
No range |
User units |
No default |
The value of the period of a cyclic system expressed in User units. The parameter is defined to correctly manage the periodicity (modulo) of the input values. |
|
Speed |
LREAL |
No range |
User units |
No default |
Sets the Axis Speed. See Set the Axis Block Position Units for more information. |
|
UserUnitPerTurn |
LREAL |
No range |
User units |
No default |
Define the unit equivalent to one revolution of the physical motor. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
No range |
N/A |
Returns TRUE when the function successfully executes. See Pipe Network - General Rules for more information. |
Remarks
- Returns TRUE if the function succeeded.
- The axis object can be mapped to servo or stepper drives.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisInit( PipeNetwork.Axis1, 360.0, 360.0, SHL(1,20), 500.0, 100000.0, 100000.0, 0.0, true ) ;