MLBlkCreate
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Creates a new Pipe Block object.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Name |
STRING |
No range |
N/A |
No default |
Designated name for the newly created Pipe Block. |
|
Type |
STRING |
No range |
N/A |
No default |
The type of Pipe Block to create. Examples: MASTER, GEAR, PHASER, etc. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
ID |
DINT |
|
|
Assigned ID number of the created Block. |
Remarks
- Before a Pipe Block is Initialized, the function needs to be created and assigned an ID number.
- The MLBlkCreate function is automatically called if a Block is added to the Pipe Network.
-
-
Pipe Blocks are normally created in the Pipe Network using the graphical engine.
You do not have to add MLBlkCreate function blocks to their programs.
The code with MLBlkCreate commands are automatically generated and called in a program with Pipe Network(MLPN_CREATE_OBJECTS).
-
-
This function should be called after MLMotionInit is called and before MLMotionStart is called.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Create a new GEAR Pipe Block named “MyGear”
MyGear := MLBlkCreate( 'MyGear', 'GEAR' );
See Also
- MLAxisInit
- See Step 3 in Initialize and Start a Pipe Network.