MLBlkIsReady
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Verifies if a Pipe Block currently has a function running.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of a created Pipe Block. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
N/A |
N/A |
Returns TRUE if no function of a specified Pipe Block is running. See Pipe Network - General Rules for more information. |
Remarks
- Returns TRUE if no function of a specified Pipe Block is running.
- Returns FALSE if the selected Pipe Block has a function running.
- Same return value as the .Q output of a specific function itself.
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller for more information.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Check if the MST Pipe Block named “MASTER” has a function running
IsReady := MLBlkIsReady( PipeNetwork.MASTER );
See Also