MLBlkReadOutVal
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Gets the output value of a selected Pipe Block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of a created Pipe Block. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Value |
LREAL |
|
|
Current output value of the selected Pipe Block. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller for more information.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Save the output of a Gear Pipe Block
BlockOutput := MLBlkReadOutVal( PipeNetwork.MyGear );
See Also