MLMstRel
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Performs a relative move for a specified distance from the current position.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
EN |
BOOL |
0, 1 |
N/A |
No default |
Enables the FB to be executed. |
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of the Master Block. |
|
DeltaPos |
LREAL |
No range |
User units |
No default |
Relative distance to the move. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
|
|
Returns TRUE when the function successfully executes. See Pipe Network - General Rules for more information. |
Remarks
None
FBD Language Example
FFLD Language Example
-
-
A pulse contact is required to start the FB.
IL Language Example
Not available.
ST Language Example
MLMstRel( PipeNetwork.MASTER, 750.0 );
See Also