MLPmpReadAccel
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Gets the Acceleration parameter of a PMP block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of a PMP function block in the Pipe Network. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Acceleration |
LREAL |
|
User unit/sec2 |
Present Acceleration of the PMP Pipe Network function block.
|
Remarks
Used in both the MLPmpAbs and MLPmpRel function blocks.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
PmpAccelValue := MLPmpReadAccel( PipeNetwork.PmpMaster ) ;
See Also