MLSyncWriteDeltaS
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Sets the output phasing value of a synchronizer block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of the Pipe Network Block. |
|
DeltaS |
LREAL |
No range |
User units |
No default |
Slope to be used during Start and stop of Synchronization. This parameter is used in MLSyncStart and MLSyncStop. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
|
N/A |
Function block executed successfully. See Pipe Network - General Rules for more information. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller for more information.
- Returns TRUE if the function succeeded.
- Output phasing is the distance or the slope the output takes to synchronize with the input when MLSyncStart block is executed.
- It also affects the distance or the slope the output takes to de-synchronize with the input and come to a stop when MLSyncStop block is executed.
Figure 6-201: Set output phasing after MLSyncStart
Figure 6-202: Set output phasing after MLSyncStop
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLSyncWriteDeltaS( PipeNetwork.SYN, 45 );