SigID
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Get the identifier of a Signal resource.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
SIGNAL |
STRING |
|
|
|
Name of the signal resource. Must be a constant value. |
|
COL |
STRING |
|
|
|
Name of the column within the signal resource. Must be a constant value. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
ID |
DINT |
|
|
ID of the signal to be passed to other blocks. |
Remarks
- Some blocks have arguments that refer to a signal resource.
- For all these blocks, the signal argument is materialized by a numerical identifier.
FBD Language Example
FFLD Language Example
IL Language Example
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them 'MySignal'
SigID 'FirstColumn'
ST ID
ST Language Example
ID := SigID ('MySignal', 'FirstColumn');
See Also