find
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Find the position of characters in a string.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
STRING |
|
|
|
Character string. |
|
STR |
STRING |
|
|
|
Specific characters to search for within the STRING. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
POS |
DINT |
|
|
|
Remarks
- The first valid character position is 1.
- The search is case sensitive.
- The return value can be used with other string functions (e.g., mid or right).
FBD Language Example
FFLD Language Example
- In the FFLD
"Free Form Ladder Diagram" Language, the operation is executed only if the input rung (EN) is TRUE. - The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
- In the IL
"Instruction List"
This is a low-level language and resembles assembly Language, the first input (the string) must be loaded in the current result before calling the function.- The second argument is the operand of the function.
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them IN
FIND STR
ST POS
ST Language Example
POS := FIND (IN, STR);
See Also