mid
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Extract characters of a string at any position.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
STRING |
|
|
|
Character string. |
|
NBC |
DINT |
|
|
|
Number of characters to extract. |
|
POS |
DINT |
|
|
|
Position of the first character to extract. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
STRING |
|
|
String containing the first NBC characters of IN. |
Remarks
- The first valid character position is 1.
FBD Language Example
FFLD Language Example
- In the FFLD
"Free Form Ladder Diagram" Language, the operation is executed only if the input rung (EN) is TRUE.- The output rung (ENO) keeps the same value as the input rung.
- The function is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
- In the IL
"Instruction List"
This is a low-level language and resembles assembly Language, the first input (the string) must be loaded in the current result before calling the function. - Other arguments are operands of the function, separated by comas.
Op1: LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them IN
MID NBC, POS
ST Q
ST Language Example
Q := MID (IN, NBC, POS);
See Also