Read the Output of a MC Function Block in ST

In this example:

A6_Inst_MC_MoveRelative( 1, Axis6, -90, 5, 300000, 300000, 0, 0 );

The syntax to read one of the outputs in STClosed "Structured text" A high-level language that is block structured and syntactically resembles Pascal for this instance is:

      <FUNCTION BLOCK NAME>.<OUTPUT>
    

This FB has these 5 outputs: Busy, Active, CommandAborted, Error, and Error ID (e.g., the Active output has this ST expression: A6_Inst_MC_MoveRelative.Active).

Example 1

UserVariable1 := A6_Inst_MC_MoveRelative.Error ;

Example 2

      IF A6_Inst_MC_MoveRelative.Active THEN
UserVariable2 := 1 ;
ELSE
UserVariable2 := 0 ;
END_IF;