Axis tab
You can view a visual representation of the motors from the Axis tab. The axis wheels are visible after your application is started. The following can be monitored from the display:
- Real and Simulated axes
- Actual position with solid line and actual position value
- Command position with the dotted line and (command position value) in parentheses
- Axis State: Powered-off , Powered-On, or Error as well as Simulated Powered Off and ON
- Identify the axes from the label, as defined by the axis name in your application
- Axis status or positions snapshot
| Information that is available by clicking on the axis | |||
|---|---|---|---|
| Title | Image (PN axis) | Image (PLCopen axis) | Image (digitizing axis) |
|
See the Axis Pipe Block section of the KAS-IDE |
See Axis Parameters in the KAS-IDE documentation for information about the axis parameters. |
||
Additionally, if an axis is in error, the error can be cleared by clicking the text below the axis title.