Backup and Restore tab
The controller can backup and restore EtherCAT
***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs devices on an EtherCAT network.
This feature:
- Is useful as a maintenance operation to replace any controller drives in an operational machine.
- Reduces the manual steps for saving/loading each drive’s firmware and parameters into a few automated steps.
The Backup/Restore functionality is located in the controller's Web server and is accessible from a web browser.
See these topics for more information:
See the Controller Backup and Restore in the KAS-IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger help.