Plugging a probe from the Pipe Network
A probe (variable) can be directly plugged or mapped to the Oscilloscope from the Pipe Network:
- Right-click on a Pipe Block
- Select Plug on channel… in the menu

- Define the probe parameters.
-
-
To enable the Plug on channel… dialog box, the KAS-IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger must be connected to the device first!
Figure 5-58: Plugging a Probe from the Pipe Network
|
Field |
Description |
|---|---|
|
Channel |
Channel's number where the variable has to be plugged |
|
Data |
Desired variable information to show (the list depends on the type of Pipe Block. See Pipe Block Descriptions for more information. |
|
Derivation Order |
Performs a derivation of the measurement of the selected variable. If this value is different from 0 (zero), the derived value of the selected order is shown on the selected channel. |
|
Derivation Period |
Specifies the modulo period for a periodic variable to remove spikes in the display of derivative orders greater than zero. The value entered should either be 0.0 (No Modulo) or the Modulo Period (e.g., 360.0). |
|
Name |
Variable's name. |
|
Type |
Variable's type. |